ADP1047 EVB connection issue

HI,

I am testing ADP1047 EVB and the ADP1047 output connect to a DC to DC.(Phase-shift).

Now I find out that the Communication is very easy to lost when the DC to DC stage turn on.

Is there any way to avoid the GUI to lost the communication with ADP1047 EVB?

  • There is just too much noise on the I2C lines and that is why the connection is lost. This is typically the case when you have a change in the system such as a load step or just when you start the PSU. This could also be aggravated by large ground loops in the layout.

    What you can do is to keep the GUI on a screen which does not have any readbacks such as the main window or the output voltage window for example. Windows to avoid are the flags and readings window.

    After the system is in steady state you can go to the flags and readings window.

    Another alternative is to put a common mode choke on the I2C adapter if you don't have one already.

    Lt Comm Data.

  • 0
    •  Analog Employees 
    on Aug 2, 2018 3:09 PM over 2 years ago
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin