ADM7154-04 max outptut volatage?

Hi all,

I'm building test boards for some RFIC's and considering ADM7154-04 as a power supply for 1.2V and 3.3V rails.

But, since these are test boards, I have to test IC's with power supply which varies +- 5%.

So, for +5%  of 3.3V is 3.465V. 

In the data sheet of ADM7154 is stated that maximum output voltage is 3.4V.  Is this internally limited or I could make it to produce 3.465V using external resistors?

I don't want to use ADM7151.

Regards,

Novica