Hello,
I'd like to ask about a Pin Connection of LTM4671.
(1) If I don't want to use a temperature monitor, I can connect TMON to INTVCC12.
In that case, how should I set the following two pins?
TSENSE0+/-:
TSENSE3+/-:
(2) The following information can be found on p.15 of the data sheet.
>>For parallel operation of N-channels, tie the VOUT, the FB pins and VOSNS– pins together but only hooking up one VOSNS+ (VOSNS) pin to the VOUT so that all the paralleling channels can share the same error amplifier and same top 60.4k feedback resistor.
In Figure 31 on p.31, there is a connection between VOSNS1+ and VOSNS2+.
Is this correct if I follow the diagram?
Best Regards,
Knj