Post Go back to editing

Dimming function of ADD5203

Dear Sir/Madam,

Our customer is studying with your ADD5203  in exchange for ADD5211 past you recommended.

Q-1

As for your "DC current dimming" function of page-12 on you datasheet,

Does this means 100%-80%- 60%,,,,,(reduce)can do, but 0%-20% 40%-,,,,,,,(growth) cannot do?

Q-2

If it is driven by current 100%, then what is the generation of heat? less than junction temperature without heat sink?

Thanks Kaos

  • Can you reply this question?

    Our customer is still waiting the answer to use or not !!

    Thanks

  • Hi Kaos,

    Sorry for the delay.  For some reason, your initial post didn't show up on Engineer Zone until today. 

    Q1:  No.  It can do both reduction and growth.  The reduction shown in Figure 18 was just for example.  We don't play any tricks on the customer! 

    Q2:  The total power dissipation (Pdiss) of the part is: 

         Pdiss = Vin*Iq + N * VFBx * ILED

              where Iq is the current consumption of the part (4.2mA typ)

              N = number of active sinks (between 1 and 8)

              VFBx is the average voltage on the active FBx pins.  For ILED=20mA, this will be something >0.65V (it depends on the voltage mismatch between the LED strings)

              ILED is the LED current

    For example, Pdiss might be:

         Pdiss = 12V*4.2mA + 8 * 1.0V * 30 mA = 290 mW

    This Pdiss is then used to calculate the die temperature, using the theta JA given in Table 6.  The exposed pad of the ADD5203 helps it to easily dissipate this power without heating the part beyond the thermal limits.  So in general, the internal heating of the IC is not an issue. 

    Best Regards,

    - Jon

  • Hi Jon,

    Thank you for your kindly answer.

    Here is one additional question,

    Can ADD5203 drive max 2A/1 LED by ganged FB1+FB2+.......FB8?

    Thanks Kaos

  • Hi Jon,

    Ok, Jon. I got it.

    I will recommend ADP8140 LED driver to our customer soon. Maybe we will provide the eval board also soon. Thanks.

    And as for the application note you have made, it's sounds good! I would like to see it, so pls send it to me after you finished.

    Thank you very much for your quick kindly support to me!!

    Kaos

  • Hi Kaos,

    No, the maximum current through 1 LED is 8x30mA=240mA.  For 2A of LED current, you could use the ADP8140.  Or a standalone boost converter (like the ADP1621) with some external modifications.  I am writing an app note on how to do that, but I can send you an advance copy if you are interested. 

    Best Regards,

    - Jon

  • This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin