Post Go back to editing

How does ADM693 shift the watchdog-timeout to?

Thread Summary

The user inquired about the watchdog timeout period for the ADM693 under varying VCC and temperature conditions. The support engineer provided bench test results for three samples, indicating that the timeout period varies with VCC and temperature. However, due to the age of the part, comprehensive design data and guaranteed specifications are unavailable. The engineer suggested using the ADM8693 for a well-defined watchdog timeout range.
AI Generated Content

Dear Sir/Madam,

As for your ADM693, our customer asked the following question to us.

I could not catch the answer on your datasheet.

So please let me know your comment.

The watchdog timeout period is showed min 1sec to max 2.25sec when VCC = 5V, TA = +25C.

Q-1

If VCC is shifted to 4.5V or 5.5V, then how should we think this value shifting?

eg; when 4.5V, shift min 0.9sec to max 2.15sec ? Otherwise same value?

Q-2

If TA is shifted to 0 to 70C, then how should we thinkthis value shifting?

eg; when around temp=0C, shift min 0.9sec to max 2.15sec ? Otherwise same value?

Please let me know the trend when the above conditions.

My expected reply as following chart if you have.

Thanks Kaos

Parents
  • Hi Ren,

    I explained your answer to our customer.

    But he could not satisfy your answer.

    Again The info Customer want to know

    1)the value of design WD-timeout

    Not only one sample, he needs the design value that was brought from a lot of samples.

    The value needs to include the individual variation of ADM693.

    Do you have this value?

    2)failed ADM693

    Customer met one failed ADM693 that was 2.28sec/4.5V at 25C tempereture WD timeout.

    So he needs the design data that this failed is real fail or not.

    Any comment?

    Thanks Kaos

Reply
  • Hi Ren,

    I explained your answer to our customer.

    But he could not satisfy your answer.

    Again The info Customer want to know

    1)the value of design WD-timeout

    Not only one sample, he needs the design value that was brought from a lot of samples.

    The value needs to include the individual variation of ADM693.

    Do you have this value?

    2)failed ADM693

    Customer met one failed ADM693 that was 2.28sec/4.5V at 25C tempereture WD timeout.

    So he needs the design data that this failed is real fail or not.

    Any comment?

    Thanks Kaos

Children
No Data