Dear Sirs
Datasheets for LTC3784 (p.23) and (at least) LTC7841 (p. 31) have note
" The value of the boost capacitor CB needs to be 100 times that of the total input capacitance of the topside MOSFET(s)."
But on all application schematic`s 0.1 uF capacitor is used along with top MOSFET`s HAT2169, RJK0652, RJK0305, BSC065N06.
Calculating max. MOSFET Input capacitance - 0.1uF/100 times = 1nF
MOSFET Input capacitance must be less then 1 nF for Cb=100nF.
But for all listed MOSFET`s input capacitance much bigger.
Could you comment this, please?
-- Best Regards,
Victor
Edit Notes
typo fixed[edited by: Levandovsky at 3:35 PM (GMT -5) on 7 Dec 2020]