Hi,
we use the LT3504 in a design to get four different voltages, what works great. Now I would like to reuse the design by minimal changes.
I need an output that delivers 2A instead of 1A. Does the LT3504 support connecting two outputs together for 2A output if they are at the same voltage?
(e.g. exactly same output schematic for SW4 and SW3 for 3V3, 1A; now connect the two lines together to one 3V3 out for 2A load)
Is it better to combine two outputs of the same phase or two that are 180 degrees out-of-phase? (or is both possible?)
Is a series diode in each 3V3 output necessary for this function?
Datasheet: https://www.analog.com/media/en/technical-documentation/data-sheets/3504fa.pdf
Thanks for your help
Flo91