The ADP5024 datasheet lists these variants but shows nothing different between the two.
ADP5024
Production
The ADP5024 combines two high performance buck regulators and one low dropout (LDO) regulators in a small, 24-lead 4 mm × 4 mm LFCSP to meet demanding...
Datasheet
ADP5024 on Analog.com
The ADP5024 datasheet lists these variants but shows nothing different between the two.
Hi Matt,
The two models only differ in packing quantity. The '-R2' comes in a Reel of 250 units, and the ''-R7' comes in Reel 1500.
-Jess