ADP7102 ADIsimPower input capacitor error

ADIsimPower is a very nice tool.. a real time saver.  However I noticed an error in the tool for the ADP2102.

Using parameters for input voltage of +12V the tool specified an input capacitor rated at 6.3V.  Either that, or C1 and C2 in the diagram below are incorrectly labeled (reversed).  Easy fix on this end, but might sink young players.