Hi
May we know the output drop voltage in AD660(doubler-mode) ?
We consider D-range for sink driver ICs or discrete.
We will use ADM660 for LED anode voltage.
Vin=5V OUT=10V max 100mA
Vf=4.6V(max)
LED Cathode connects to sink driver and etc.
We have Output Resistance and TPC3 characteristics in ADM660 datasheet.
These are same specification in Both Invertring Mode and Doubling Mode, aren't them?(Are SPECIFICATIONS and any graph for Both of them?)
Is ADM660 Output Resistance specification at TA = TMIN to TMAX?
Best regards
Thank you very much
Hello,
Hopefully this helps.
Thank you for your kind reply.
I mean "the output drop" is a difference between ideal Vout (2Vin) to actual Vout.
I think that the actual output depends on external C1,C2 mismatch, ESR and frequency (from datasheet p.7 p.9 ).
In Specification, it is C1=C2 and ESR<0.2ohm.
Thank you very much.