LTC4279 RPM abnormal setting

Hi,

if LTC4279 RPM is in a abnormal state.

Like Open/Short/Out of window.

What will happen?

If the fuse is necessary for the safety certificate?

Thanks a lot.

Please kindly help with this.

  • +1
    •  Analog Employees 
    on Nov 17, 2020 5:42 PM

    Set the PSE to the system required power mode by selecting a 1% resistor with a value specified for RPM in Table 1 of the LTC4279 datasheet.  Setting the LTC4279 PWRMODE pin to open, short or a value different from the table is not recommended for normal operation; the LTC4279 after reset will default to the closest power mode in Table 1 if this is done.

    A fuse is not required for IEEE 802.3af/at compliance.  However, it may required in the application to meet the applications safety requirements.