Post Go back to editing

LTC1325

Hi All,

Having issues with LTC1325. At present interfaced via 4 wire SPI with Arduino mega 2560 in prototyping stage. 

issues I have...

Vreg is not within spec shows 2.86V with no load and 12V VDD, should be 3.074v min.

Dout is also not within TTL spec ie. Vol=0.4V and Voh=2.4V, I get nothing but 200mv from that pin

Thanks in advance...

Luca

Parents Reply Children
No Data