WHEN AC ADOPTER POWER ON & OFF RAPIDLY, ADP5052 BREAK DOWN, AND MEASURE RESISTANCE OUTPUT PORT BETWEEN GND IS VERY LOWER THAN BEFORE.
OFF COURSE ,DONT WORK CORRECTLY
WHY?
ADP5052
Recommended for New Designs
The ADP5052 combines four high performance buck regulators and one 200 mA low dropout (LDO) regulator in a 48-lead LFCSP package that meets demanding performance...
Datasheet
ADP5052 on Analog.com
WHEN AC ADOPTER POWER ON & OFF RAPIDLY, ADP5052 BREAK DOWN, AND MEASURE RESISTANCE OUTPUT PORT BETWEEN GND IS VERY LOWER THAN BEFORE.
OFF COURSE ,DONT WORK CORRECTLY
WHY?
Hi Nick,
Please check if U17 IRHLS6276 is damaged? If so, please measure if Vds voltage on U17 is over the voltage rating 20V when ac adapter power on/on rapidly. Thanks.
Jun