Post Go back to editing

ADP5024 output problem

Hello, I am having an issue with the switching outputs on a new board with ADP5024.

Expected:

VOUT2 =1.8V

SW2 switches from 0~5V (VSYS) at 36% duty cycle, at 3MHz.

Actual:

VOUT1 ~100mV

SW2 switches from -1~4.5V at 20% duty cycle, at 1.5MHz

My schematic is below and is largely similar to the one from the BF707 EZKIT.

Any troubleshooting tips would be appreciated.

matt

Parents Reply Children
No Data