Hello, I am having an issue with the switching outputs on a new board with ADP5024.
Expected:
VOUT2 =1.8V
SW2 switches from 0~5V (VSYS) at 36% duty cycle, at 3MHz.
Actual:
VOUT1 ~100mV
SW2 switches from -1~4.5V at 20% duty cycle, at 1.5MHz
My schematic is below and is largely similar to the one from the BF707 EZKIT.
Any troubleshooting tips would be appreciated.
matt