Post Go back to editing

ADP5024 output problem

Hello, I am having an issue with the switching outputs on a new board with ADP5024.

Expected:

VOUT2 =1.8V

SW2 switches from 0~5V (VSYS) at 36% duty cycle, at 3MHz.

Actual:

VOUT1 ~100mV

SW2 switches from -1~4.5V at 20% duty cycle, at 1.5MHz

My schematic is below and is largely similar to the one from the BF707 EZKIT.

Any troubleshooting tips would be appreciated.

matt