LTC3251-1.2 Connection Doubt

Hello,

I am carrying out an own design that embeds the LTC3251-1.2 device.

As I can see in the datasheet, both MD0 and MD1 are able to configure the operation mode of the device, in the attached figure named "LTC3251-1.2_connection" you can see  the typical application getting from your datasheet. But you not show the MD1 and MD0 Voltage leven in any moment.

If I keep seeing the datasheet, there is a Table which shows the typical operation ratings for the device. In the attached figure named "LTC3251-1.2_pins Ratings" you can see the ratings values for both MD0 and MD1.  And you can see how the maximu voltage value is 1.2V. For this reason I have a question:

- I can not understand how I have to supplied 1.2 V in these pins when I am using this part to get this voltage level. So, it is possible to supplied the MD1 and MD0directly with Vin(5V) voltage? or have i to decrease the voltage by a resistor divider?. because i guess that i can not connect the pin Vout directly with MD0 or MD1, I mean, I can not design a feedback connection between them.

By the way, ther is a reference design in you web about the LTC3251 device (also attached as LTC3251). And as you can see MD0 and MD1 pins can be supplied directly by Vin.

Parents Reply Children
No Data