Post Go back to editing

ADP5585 going BAD after few days usage.ESD ISSUES?

We are using ADP5585 in our design for interfacing to a keyboard. The schematics is as shown in the attachment. The lines KBC0,1,2,3 and KBR0,1,2,3 are going to a 4 X 4 matrix KEYPAD connected with about 15 inches long ribbon cable.

The capacitors C2,C4,C6,C8, C67,C68,C69,C74 though are shown in schematics are not really mounted on board.

The device TPD8F0003DQDR is being used as ESD protection device Its link is http://www.ti.com/lit/ds/symlink/tpd6f003.pdf

we are noticing that in spite of using above ESD protection device we are seeing failures of the ADP5585 device. The failed devices basically have less than 50 ohm resistance between any of the I/O pins and GND. Incidentally we are seeing that even the lines which are not connected to KEYPAD like pin numbers 16, 10 and 1 which are connected to internal signals also develop this low resistance between that specific pin and GND.

Also these failures Occur only after a few days of usage typically 5-10 days with KEYPAD being used about 10-15 times per days

Following questions

1. Has anyone else or even Analog devices have seen these kind of failures happening with ADP5585

2. Is there any other issues in the schematics attached ?

3. Is there really a ESD issue or is it for any other reason that the ADP5585 device may be going bad ?

4. Should we use any other ESD protection device than the currently used ? probably the clamping voltage of the device we are using is little bit higher than the transient tolerance limit of ADP5585

Parents
  • The ADP5585 family has very good ESD protection within the part, and we haven't seen ESD issues that I know of.

    A 15 inch ribbon cable can sometimes come with a lot of capacitance, which could slow down the polling on the keypad key scans, but this would not cause the part to short to ground.

    When the failure happens, does the part operate correctly the next time it is powered up, or is the pin permanently weakly shorted to ground?

    Just to make sure, are the voltages from the CPU also 3.3 V? What is the KP_12V_OFF line connected to?

    C2,C4,C6,C8, C67,C68,C69, and C74 should remain unpopulated as they aren't necessary, and can actually interfere with the key polling.

    Is there any chance the chassis ground is different from the IC ground? Could there be a large voltage spike that could couple into the row and column pins somehow?

    RSchnell

Reply
  • The ADP5585 family has very good ESD protection within the part, and we haven't seen ESD issues that I know of.

    A 15 inch ribbon cable can sometimes come with a lot of capacitance, which could slow down the polling on the keypad key scans, but this would not cause the part to short to ground.

    When the failure happens, does the part operate correctly the next time it is powered up, or is the pin permanently weakly shorted to ground?

    Just to make sure, are the voltages from the CPU also 3.3 V? What is the KP_12V_OFF line connected to?

    C2,C4,C6,C8, C67,C68,C69, and C74 should remain unpopulated as they aren't necessary, and can actually interfere with the key polling.

    Is there any chance the chassis ground is different from the IC ground? Could there be a large voltage spike that could couple into the row and column pins somehow?

    RSchnell

Children
No Data