In my application I would like to use it to drive a high impedance input, and the pull up current for the open drain is significant compared to the rest of my circuit.
ADCMP380
Recommended for New Designs
The ADCMP380 is an ultralow power voltage comparator with internal reference suitable for use in general-purpose applications. The ultralow power consumption...
Datasheet
ADCMP380 on Analog.com
In my application I would like to use it to drive a high impedance input, and the pull up current for the open drain is significant compared to the rest of my circuit.
I see.
I can't help you with the push pull situation, but I may have a solution to make your divider dream come true.
take a look at ADM8611.being voltage supervisors they operates slightly different to compactors in that they have a build in delay. but i don't see that being a issue for your application.
note not all threshold options are available in production, in fact only 2.63V is currently available for ADM8611, there's a also 2.32V on ADM8613. they may work with your 3V battery.
Ren
I see.
I can't help you with the push pull situation, but I may have a solution to make your divider dream come true.
take a look at ADM8611.being voltage supervisors they operates slightly different to compactors in that they have a build in delay. but i don't see that being a issue for your application.
note not all threshold options are available in production, in fact only 2.63V is currently available for ADM8611, there's a also 2.32V on ADM8613. they may work with your 3V battery.
Ren