Hi,
I use LTC4359 as a power switch and input reverse protection.

Recently I had two boards in which the NMOSFET Q1A was short between drain and source.
Do I have to put an inrush control circuit (C1 and R4)on the GATE, as shown in Figure 6 in LTC3459 datasheet ?
My input voltage is 6.4V~8.4V, the maximum output current is 800mA.
Thank you,
Brook