hello
I see in the datasheet that the LT3010 is used to power INT_vcc. May I ask whether the GND of LT3010 is connected to SGND or PGND

BI1IZF
KCC's Quizzes AQQ306 about a fish stick challenge
1. First the quote of the month: " I am so clever that sometimes I don't understand a single word of what I am saying" - Oscar Wilde
2. New quiz AQQ306 about a fish stick challenge:
Here below is a pseudo fish diagram swimming to the right.
Question
View All
October Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Finding Your Circuit Chi — EMC Quiz!
Think you know EMC? Test your knowledge with our 5-question quiz!
Read the blog first, then take the challenge: Finding Your Circuit Chi
Every current flowing creates electromagnetic fields.
Strong EMC design
View All
LT3010
Recommended for New Designs
The LT3010 is a high voltage, micropower low dropout linear regulator. The device is capable of supplying 50mA output current with a dropout voltage of...
Datasheet
LT3010 on Analog.com
LTC4020
Recommended for New Designs
The LTC4020 is a high voltage power manager providing PowerPathâ„¢ instant-on operation and high efficiency battery charging over a wide voltage range...
Datasheet
LTC4020 on Analog.com
hello
I see in the datasheet that the LT3010 is used to power INT_vcc. May I ask whether the GND of LT3010 is connected to SGND or PGND

BI1IZF
I am glad you asked this question because the use of the INTVcc preregulator in datasheet figure 9, figure 10 and the application circuit on p. 39. will not work. Please use the following circuit instead. Note that I have connected the ground pin of the LT3012 to PGND.
I used the LT3012 which can supply 250mA; the LT3010 can supply 50mA.

Hello.
To be honest, I'm a little confused. What is the reason why the circuit will not work in datasheet on p. 39? Because a low power regulator (LT3010) is used? Or is it not the correct wiring diagram? As I can see from your figure, you connected the regulator output to the PVIN and INT_Vcc pin of LTC4020. But, according to the block diagram on page 14 of the datasheet, pin PVIN is an input, and INT_Vcc is an output. And in your circuit they are shorted. It is correct?
After reading a few more topics on the forum, I found the following recommendation for connecting an regulator .
Recomendation from ADIApproved
As we can see from the figure, the regulator is connected only to the PVIN pin. And the INT_Vcc pin is connected only to the anodes of the diodes that power the transistor driver. This connection allowed the internal INT_Vcc regulator to do its work with a lower input voltage. But still maximum current is limited by 150 mA value.
If connect the transistor drivers (BST1, BST2) not to the INT_Vcc pin (via diodes), but directly to the LT3012 (shown in the figure)? Will this be correct? In this case, there will be no short circuit between the INT_Vcc pin and PVIN of LTC4020 , and the entire power load for the transistor drivers is completely loaded on the LT3012.

Sorry for my english, best regards.
Hello.
To be honest, I'm a little confused. What is the reason why the circuit will not work in datasheet on p. 39? Because a low power regulator (LT3010) is used? Or is it not the correct wiring diagram? As I can see from your figure, you connected the regulator output to the PVIN and INT_Vcc pin of LTC4020. But, according to the block diagram on page 14 of the datasheet, pin PVIN is an input, and INT_Vcc is an output. And in your circuit they are shorted. It is correct?
After reading a few more topics on the forum, I found the following recommendation for connecting an regulator .
Recomendation from ADIApproved
As we can see from the figure, the regulator is connected only to the PVIN pin. And the INT_Vcc pin is connected only to the anodes of the diodes that power the transistor driver. This connection allowed the internal INT_Vcc regulator to do its work with a lower input voltage. But still maximum current is limited by 150 mA value.
If connect the transistor drivers (BST1, BST2) not to the INT_Vcc pin (via diodes), but directly to the LT3012 (shown in the figure)? Will this be correct? In this case, there will be no short circuit between the INT_Vcc pin and PVIN of LTC4020 , and the entire power load for the transistor drivers is completely loaded on the LT3012.

Sorry for my english, best regards.