hello
I see in the datasheet that the LT3010 is used to power INT_vcc. May I ask whether the GND of LT3010 is connected to SGND or PGND

BI1IZF
LT3010
Recommended for New Designs
The LT3010 is a high voltage, micropower low dropout linear regulator. The device is capable of supplying 50mA output current with a dropout voltage of...
Datasheet
LT3010 on Analog.com
LTC4020
Recommended for New Designs
The LTC4020 is a high voltage power manager providing PowerPathâ„¢ instant-on operation and high efficiency battery charging over a wide voltage range...
Datasheet
LTC4020 on Analog.com
hello
I see in the datasheet that the LT3010 is used to power INT_vcc. May I ask whether the GND of LT3010 is connected to SGND or PGND

BI1IZF
I am glad you asked this question because the use of the INTVcc preregulator in datasheet figure 9, figure 10 and the application circuit on p. 39. will not work. Please use the following circuit instead. Note that I have connected the ground pin of the LT3012 to PGND.
I used the LT3012 which can supply 250mA; the LT3010 can supply 50mA.

Thanks for answering,
I did not use PowerPathFET,
So how should my FBG pin be connected?
Is it better to use LT3010 or LT3012?
Thanks for answering,
I did not use PowerPathFET,
So how should my FBG pin be connected?
Is it better to use LT3010 or LT3012?
Following is more explanation on FBG and DC2044A schematic.
For CC/CV mode a powerpath FET is used to disconnect the battery after timeout. The voltage divider connected from the battery is returned to FBG. After timeout FBG is disconnected from ground (internal to LTC4020), so the voltage divider does not drain current from the battery. This is why the DC2044A uses the FBG connection instead of SGND for the voltage divider.
For Lead-Acid mode no powerpath FET is necessary because the charger operates continuously (trickle charge). It is OK to use SGND for the voltage divider return, because the charger operates continuously.