Post Go back to editing

Startup issue ADP5090

Hello all,

I'm having an issue with the ADP5090 startup sequence with some of my PCB's. Some of our PCB's came back not working. I use the ADP5090 to charge and manage a small 25 mAh Lithium polymer battery and use RFID Vout to as Vin for the ADP5090. This works fine on most of the PCB's but some the ADP5090 never achieves a stable SYS voltage as shown in the measurement below:

Note: Voltages are a bit higher than in real life due to max setting on scope.

More zoomed in on the issue. SYS reaches a good voltage but than collapses back to the End of Cold-Start Operation Threshold.

This is the schematic used:

Hope anyone can point me in the right direction of this issue.

Thanks,

Michael

Parents
  • Hi Kevin,

    Ok I'm going to try that. I was wondering though how is it possible that SYS voltage has such a voltage drop when the battery is connected. The battery has zero voltage drop when PGOOD comes high. Isn't the battery connected to SYS when PGOOD is high?

    Also wanted to share this image regarding the voltage drop and PGOOD

Reply
  • Hi Kevin,

    Ok I'm going to try that. I was wondering though how is it possible that SYS voltage has such a voltage drop when the battery is connected. The battery has zero voltage drop when PGOOD comes high. Isn't the battery connected to SYS when PGOOD is high?

    Also wanted to share this image regarding the voltage drop and PGOOD

Children
No Data