Post Go back to editing

LT1944: output voltage fixed multiple of input

Thread Summary

The user inquires about using the LT1944 to achieve a 16V/10mA output and a second output that is 1.5x the input voltage (3-4.5V) with a max current of 100mA. The final answer indicates that the current limit of 250mA makes it impossible to achieve 16V/100mA from a 5V input. The user is advised to use LTspice to verify design changes or consider other boost regulators. Relevant Analog Devices products: LT1944, micropower boost regulators.
AI Generated Content

I am working on a design using LT1944, with input of 2-3V and the first output of 16V/10mA max.  The second output I would like to set at a fixed multiple of the input voltage (1.5x), so it varies from 3-4.5V according to the input.  Max current from that output would be 100mA.  So in essence, not unlike a charge pump function.  Would this be possible?

Regards,

Jon

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.