Hi all!
I want to get 3V output using ADP151ACPZ-1.8 in adjustable output voltage operation mode.
My schematic is:
But I'm not sure about EPAD pin connection. Could I connect EPAD pin to PCB ground. Or I must connect it to GND pin of ADP151?
ADP151
Production
The ADP151 is an ultralow noise, low dropout (LDO) linear regulator that operates from 2.2 V to 5.5 V and provides up to 200 mA of output current. The...
Datasheet
ADP151 on Analog.com
Hi all!
I want to get 3V output using ADP151ACPZ-1.8 in adjustable output voltage operation mode.
My schematic is:
But I'm not sure about EPAD pin connection. Could I connect EPAD pin to PCB ground. Or I must connect it to GND pin of ADP151?