Post Go back to editing

VIOC-Pin at the LT3094

Hello,

I have a question about the VIOC-Pin at the LT3094. Currently I am using the TPS65131 from Texas Instruments as a DC-DC-Converter. I have connected the LT3094 as a post-regulator at the negative output of the DC-DC-Converter. The positive output is connected to the LT3045. Unfortunately the LT3094 gets warmer than the LT3045. I suggest that this is caused because the VIOC-Pin at the LT3094 is not connected to the negative Feedback-Pin of the DC-DC-Converter. The resistor values are calculated from voltage at the Feedback Pin but at the DC-DC-Converter its typically 0 V, so I am not able to calculate the values. Currently the LT3094 converts the -15 V from the DC-DC-Converter to -12 V. 
How do I connect the VIOC-Pin to the DC-DC-Converter?
Thank you !
Yours sincerely
Seeran Raveendran
Parents Reply Children
No Data