Post Go back to editing

LT3045(-1) and LT3094 - can those work with >15V output (but no more than absolute rating of 16V)?

Hi,

From what I see in datasheet of LT3045/LT3045-1/LT3094 output voltage is up to 15V. Absolute maximum rating is 16V on any of pin (OUT, OUTS). In my application I need slightly higher voltage, ideally 16V, but still do not want to stress device to absolute maximum rating. Would it work with output set to 15.5 or 15.7V? 

Thank you in advance for your help,

Artur