Hello,
At what temperature does the temperature protection circuit built into the LT3693 operate?
And at what temperature does the LT3693 restart?
Best Regards,
LT3693
Production
The LT3693 is an adjustable frequency (200kHz to 2.4MHz) monolithic buck switching regulator that accepts input voltages up to 36V. A high efficiency 95mO...
Datasheet
LT3693 on Analog.com
Hello,
At what temperature does the temperature protection circuit built into the LT3693 operate?
And at what temperature does the LT3693 restart?
Best Regards,
Hi,
Thanks for the application of LT3693.
In LT3693, the trigger temperature of the thermal protection is 165 degree Celsius.
After the thermal protection, the part restarts at 160 degree Celsius.
Best regards,
Andrew
Hi,
Thank you for your reply.
Best Regars,