Hello everybody,
I use the ADP5061 as battery management IC on a prototype. The board is powered via USB-C with a fixed configured current limit of 3A. The VINx current limit feature of the ADP5061 is therefore not required. My system draws a current peak of 1.2A for 500us at bootup. The default current limit feature of the ADP5061 limits the current to 500mA, preventing the host controller from booting. (ADP5061ACBZ-2-R7 DIG_IO1 = High) As a result, the ADP5061 cannot be configured for a higher limit, as the I2C connection is not yet established.
Is there a workaround for this deadlock constellation that requires no additional components? For example a higher default current limit? The planned product does not run in high quantities (in the hundreds of pieces) therefore a factory programming is probably not worthwhile. I would not like to use a new IC, as I am otherwise very satisfied with the performance.
Many thanks!