Post Go back to editing

Pin compatible with LTM8023

Hi,

I have  a LTM8023 on a PCB but am in need of a higher supply current than it can deliver. Is there a pin compatible device that I could use with a higher maximum Iout (e.g. 4A instead of 2A) that has exactly the same pin configuration so I would not have to change anything on the PCB?

BR

Frederikke

Parents Reply Children
No Data