Post Go back to editing

3kV flyback design with LT8302

Hello,

Actually I want to design a 3kV/4W generator.I don't want to generate 3kV directly at the out of the flyback transformer (Because of the size of the transformer) but to generate 1.5kV and to add a voltage doubler.

Without the voltage doubler I have 1.5kV at the output. When I add the voltage doubler the voltage is not multiplied by 2 (In fact at the secondary we dont have a symetric voltage) and more the voltage at the secondary is weaker with 50nF in the voltage doubler and 4500V with 10nF in the voltage doubler.

I don't find how to design a flyback power with voltage doubler (Because I think that the impedance of the voltage doubler is most important to design the flyback DCDC), do you have informations, a paper, or recommendation ?

Input parameters to design it :

Vin : 3.7V - 4.2V

Vout : 3000kV

Pout : 4W

Non isolated

Best Regard's

LT8302_1500V.asc

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.