ADP2291 dont indicate for charging the battery

Hi Folks,

I am Using the ADP2291 . I have two circuits parallel which they are Isolated with BAT1000 to support the system .

 I am using Sanyo Battery 18650(4.1~3.7 V ,2800mA).

I used the application circuit with HERMAL PROTECTION, figure 25 on data sheet .

The only difference is RS value which is 0.15 ohm to increase the charging current at the beginning .

Single circuit ,(100% Discharged Batt)Power up the circuit will draw 1500 mA as expected . after 10 minutes Led goes to off mode. Input current draw by source is reaching to 400 ma after 15 min .  I expect to charging continue for at least 2 hours with approximately 1300 mA  to full charge the battery .

input voltage is 5.04 v---4.74 V is the voltage before on RS In-Pin  ,100 mV drops cross the RS .  VCE = 0.922 ---VB =3.74V

V ADJ = 2.145v

V CHG = 3.69  ,V between the Resistor and LED is 3.69 V ...No current drawn .

Note : I placed the NTC close to the Pin of the Batt . Temp of the battery is not exceed the 95 degree F (Measured )

 Why the circuit goes to shutdown status very quick ?

Picture is attached .

Thanks for Help

Ash

Parents
  • 0
    •  Analog Employees 
    on Aug 2, 2018 3:38 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Reply
  • 0
    •  Analog Employees 
    on Aug 2, 2018 3:38 PM
    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
    EZ Admin
Children
No Data