Post Go back to editing

Parallel connecting LT1850 for higher current

Hey All,

I wish to step-down 12V 100A to 8.1V would this be possible by parallel connecting two LT1850. The datasheet suggests using dual outputs to source upto 50A which is 25 per channel. Running 50A per channel would increase the Tja beyond specification. My spec are as follows

  • Vin: 12V
  • Vout: 8.1V
  • Frequency: 400kHz
  • Duty cycle: 0.675

Thanks in advance.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.