Post Go back to editing

Need BAcklight LED Driver

Hello Support team,

Currently we are looking for a suitable Backlight LED driver to be designed for our display application.

Requirement specs are as below:

For DAY mode, operating voltage is 28.5V +/- 0.5V and operating current is 50mA and

For NIGHT mode, operating voltage is 26.5V +/- 0.5V and operating current is 5mA

Backlight LED circuit consists of 2 series and 5 parallel LEDs and we have been provided only two pin connector to drive these LEDs.

Input voltage: 12V +/-10%

Dimming method: PWM preferred

Could you please suggest few efficient and economical LED drivers to meet the above requirements.

Thanks & Regards,

Rajesh Kumar

Parents Reply Children