Post Go back to editing

Need advice on choosing the best IC for LED driver with 40 Ampere output current

I'm Jurgen from Germany. I'm a LED driver designer and designed LED drivers up to 1kW. Now I face a heavy challenge as follows:

UIN is 10V to 60V DC

IOUT is 40 A; in steps of 0%, 25% (10A), 50% (20A), 75% (30A), 100% (40A).

LED is 3.5V at 40A max.

I checked a lot of drivers, eg. LT8391A or LT3763.

I think, 40A output current is really at the edge of possible single-stage solutions.

My thoughts are to use  a synchrone current controller, and / or 2-stage controller.

Can somebody give me more hints or ideas, about solutions to deliver this huge output current?

Thank you very much!

Jurgen.

Parents Reply Children
No Data