Post Go back to editing

Temperature rise on LTC3815

I was doing thru the app note you’ve written – Design Note 554 for LT3815. I’m highly impressed with this unique flyback converter and planning on using it for my upcoming design.

However, I’m concerned about the temperature rise on my board if I had to use this converter at high temperature operations. I understand that LT8315HFE is rated up to 150C, but my ambient conditions would be high temperature (150C). I’m looking to use the converter for about 7W load.

Having said that, I wanted to understand what would be the temperature rise within LT3815? As per thr app note, for a nearly 11W power supply, the temperature rise was about 37C above ambient.

From datasheet Θjc is about 10C/W, but I believe that the temperature rise within flyback transformer is not directly proportional to the output wattage but dependent on the efficiency. In the example, it is mentioned that the efficiency is about 80%?

 So, I wanted to know how can I determine the temperature rise for my application? do you have any suggestions?

  • Hi bytewise,

    In datasheet or part numbers in website, I cannot see an H-grade version of LTC3815 but only E & I grades. It means that you cannot operate these parts higher than 125degC junction temperature and therefore slightly lower than 125degC ambient temperature to account for losses. Electrical Characteristics table in datasheet is qualified and therefore guaranteed only up to 125degC.

    Temperature rise guideline is in page 29 of datasheet.

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.