Hi,
I'm doing 5V to +-16.8V with this part. Less than 100mA output current. I'm noticing very high in rush current, part of the problem is the amount of output capacitance I have on the board. But I just can't seem to get the soft start to significantly reduce in rush. I've tested 4.7k / 10uF RC time constant at the input but still in-rush is between 2.5A and 3A. I'd like to get in-rush down to 0.5A. I don't care how long the supply takes to come up, 1 sec is fine. In simulation I've tried up to 100k / 10uF and I can't seem to reduce in-rush either. The enable pin starts near 1.8V always, it doesn't have a nice RC curve to it. I can't understand why this is, it should be changing at the start of simulation from near 0V to 1.8V.
I'm attaching my circuit simulation, which matches my actual board design fairly well.
Thanks for any suggestions!
Erik