Hey all,
Was wondering how i can increase current sourcing capability of the ADP1850 for 100A. Is it possible to interleave two or maybe use two in parallel to achieve this ? If not what would be a good external clock ?
ADP1850
Recommended for New Designs
The ADP1850 is a configurable dual output or two-phase, single
output dc-to-dc synchronous buck controller capable of running
from commonly used 3.3 V...
Datasheet
ADP1850 on Analog.com
Hey all,
Was wondering how i can increase current sourcing capability of the ADP1850 for 100A. Is it possible to interleave two or maybe use two in parallel to achieve this ? If not what would be a good external clock ?
Hi
I would recommend looking at LTC1629s as it has DC256A with a 90A this might be a better option on your application
Regards,
Hi
I would recommend looking at LTC1629s as it has DC256A with a 90A this might be a better option on your application
Regards,