Hey all,
Was wondering how i can increase current sourcing capability of the ADP1850 for 100A. Is it possible to interleave two or maybe use two in parallel to achieve this ? If not what would be a good external clock ?
ADP1850
Production
The ADP1850 is a configurable dual output or two-phase, single
output dc-to-dc synchronous buck controller capable of running
from commonly used 3.3 V...
Datasheet
ADP1850 on Analog.com
Hey all,
Was wondering how i can increase current sourcing capability of the ADP1850 for 100A. Is it possible to interleave two or maybe use two in parallel to achieve this ? If not what would be a good external clock ?
Hi
I would recommend looking at LTC1629s as it has DC256A with a 90A this might be a better option on your application
Regards,
Hi,
It may be possible but we have not done it. Please try to check LTC6908 (Oscillator with Spread Spectrum Modulation) and DC2253A as example of how it was used.