Post Go back to editing

LTC3886-1 Register Value Question

Dear Sir/Mamm,

I have a question two condition of LTC3886-1.   

I want to know how the register setting changes in both cases of LTC3886-1.

1. When using four independent channels of output:

2. To combine outputs into one and use four outputs,

I will use the parameter values set below.

Command Name

CMD

CODE

SET

VALUE

MFR_CONFIG_ALL_ LTC3886

0xD1

0x21

MFR_PWM_MODE_LTC3886

0xD4

0x81

OPERATION

0x1

0x80

ON_OFF_CONFIG

0x2

0x1E

VOUT_OV_FAULT_ RESPONSE

0x41

0x47

VOUT_UV_FAULT_ RESPONSE

0x45

0x47

IOUT_OC_FAULT_ RESPONSE

0x47

0x87

TON_MAX_FAULT_ RESPONSE

0x63

0x80

OT_FAULT_RESPONSE

0x50

0

UT_FAULT_RESPONSE

0x54

0

MFR_FAULT_RESPONSE

0xD5

0

MFR_PWM_CONFIG_LTC3886

0xF5

0x90

Others 

 Default




Parents Reply Children