Post Go back to editing

ADP2108, ADP5300, ADP5302 100% duty operation input voltage

Hi All,

 

One of my customer is considering to use DC-DC regulator on his prototype board.

I recommended ADP2108, ADP530, or ADP5302 for his purpose.

He sent me the following question.

What is the input voltage at which the device reaches 100 duty operation for Vout=3.0V, Iout=100mA?

 

Thank you for your help.

Ricky

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.