Post Go back to editing

ADP5585 - no communication when interrupt onHey, I have a problem with ADP5585 - I can read status value, when I press button read event fifo then clear int flag etc, but when I want to use interrupt pin - I can't even read status register - always 0,

Hey, I have a problem with ADP5585 - I can read status value, when I press button read event fifo then clear int flag etc, but when I want to use interrupt pin - I can't even read status register - always 0, device generate first interrupt and then I don't have communication with AD5585.

Register 0x38 -> 0x0f

Register 0x39 -> 0x0f

Register 0x3B -> 0x80

Register 0x3b -> default - 0, when turn 0x01 - no communication.

Did I miss something?

Parents Reply Children
No Data