Post Go back to editing

(ADR3533)What will happen if Vout short to GND?

Hi !

I have some questions about ADR3533.

Our customer are asking me this question.

Q1)

What will happen if Vout short to GND?

Would it broke the device?

Or would it be no problem?

Q2)

If the device will broke, can you explain why the device will broke?

If the device won't broke can you explain why the device won't broke?

VIN=5V

ENABLE=5V

GND_SENSE=0V

GND_FORCE=0V

VOUT_SENSE=0V

VOUT_FORCE=0V

Best regards.

Kawa

Parents
  • Hi Phil

    I measured ADR3533 Vin current when the output short to GND.

    The result was 50~60mA.

    Also the device didn't broke.

    So the wattage will be maybe 300mW.

    Junction temperature will rise 40 deg.

    So this means ADR3533 will survive if the Ta is low enough.

    Is this correct?

    I need more detail if the device will broke when the output shorted to GND.

     

    Best regards.

    Kawa

Reply
  • Hi Phil

    I measured ADR3533 Vin current when the output short to GND.

    The result was 50~60mA.

    Also the device didn't broke.

    So the wattage will be maybe 300mW.

    Junction temperature will rise 40 deg.

    So this means ADR3533 will survive if the Ta is low enough.

    Is this correct?

    I need more detail if the device will broke when the output shorted to GND.

     

    Best regards.

    Kawa

Children
No Data