Post Go back to editing

(ADR3533)What will happen if Vout short to GND?

Hi !

I have some questions about ADR3533.

Our customer are asking me this question.

Q1)

What will happen if Vout short to GND?

Would it broke the device?

Or would it be no problem?

Q2)

If the device will broke, can you explain why the device will broke?

If the device won't broke can you explain why the device won't broke?

VIN=5V

ENABLE=5V

GND_SENSE=0V

GND_FORCE=0V

VOUT_SENSE=0V

VOUT_FORCE=0V

Best regards.

Kawa

Parents
  • Hi Phil

    Also why did you say "On the other hand, if the output will be connected to ground for a long time, it will probably break the part forever."?

    Is this because temperature?

    What will happen if Ta is low enough?

    And which circuit will broke?

    Would the output stage circuit will broke?

    Best regards.

    Kawa

Reply
  • Hi Phil

    Also why did you say "On the other hand, if the output will be connected to ground for a long time, it will probably break the part forever."?

    Is this because temperature?

    What will happen if Ta is low enough?

    And which circuit will broke?

    Would the output stage circuit will broke?

    Best regards.

    Kawa

Children
No Data