Post Go back to editing

(ADR3533)What will happen if Vout short to GND?

Hi !

I have some questions about ADR3533.

Our customer are asking me this question.

Q1)

What will happen if Vout short to GND?

Would it broke the device?

Or would it be no problem?

Q2)

If the device will broke, can you explain why the device will broke?

If the device won't broke can you explain why the device won't broke?

VIN=5V

ENABLE=5V

GND_SENSE=0V

GND_FORCE=0V

VOUT_SENSE=0V

VOUT_FORCE=0V

Best regards.

Kawa

Parents
  • Hi Kawa-san,

    I have to correct my statement on my previous reply. The 10 mA is minimum spec not maximum, I overlooked the number here. The maximum current can be very much higher than 10 mA.

    On the other hand, if the output will be connected to ground for a long time, it will probably break the part forever.

    Regards,

    Phil

Reply
  • Hi Kawa-san,

    I have to correct my statement on my previous reply. The 10 mA is minimum spec not maximum, I overlooked the number here. The maximum current can be very much higher than 10 mA.

    On the other hand, if the output will be connected to ground for a long time, it will probably break the part forever.

    Regards,

    Phil

Children
No Data