Post Go back to editing

Is there Spice model for ADP3624?

Looking for spice model for ADP3624 model to do some simulation and testing.

Parents
  • Hello,

    The ADP3654 is not meant for continuous operation at 2A current. It will not be able to sustain a DC current of 2A for long and will get hot. It will still be able to sustain it in my opinion but a more elegant solution is to simply use a V to I converter.

    Feed the 0-20mA into a resistor, say 1 ohm,  to create a voltage, feed that into a V to I using an op amp (any ADI opamp with 5V rating will do). You'll need to put a sense resistor on the low end of your load for this to work.

    Lt. Comm Data

Reply
  • Hello,

    The ADP3654 is not meant for continuous operation at 2A current. It will not be able to sustain a DC current of 2A for long and will get hot. It will still be able to sustain it in my opinion but a more elegant solution is to simply use a V to I converter.

    Feed the 0-20mA into a resistor, say 1 ohm,  to create a voltage, feed that into a V to I using an op amp (any ADI opamp with 5V rating will do). You'll need to put a sense resistor on the low end of your load for this to work.

    Lt. Comm Data

Children
No Data