ADP7104 and ADP151 input and output Capacitor

Dear support,

in my design I use ADP7104 and ADP151 linear regulator.

In the figure 2 on pag.1 of the ADP7104 datasheet it reports an Electrolytic Capacitor, if I correctly understand,

but on pag. 17 of the datasheet, it is written that ceramic capacitor can be used in input and output of the device.

This is also regarding the ADP151.

My question is, can I use 1uF ceramic capacitor instead of electrolytic?

If yes, could you suggest the best manufacturer model for this ceramic capacitor?

Thank you in advance for your help

Luca