Hi Team,
the goal of my project is to design a Dc/Dc Converter to supply DC Motor
The DC/DC Converter has this requirements:
Vin:9-32V
Vout: 48V
Iout:12A max
I have tried several IC (Boost Converter,Synchronous) but I would like your suggestion.
The IC LTC3779 can it be suitable for the application? Naturally, as it is a buck-boost, it would only be used as a boost.
I could buy the eval DC2654A but I don't Know if the suitable demo as the Vin min is 16V (not lower)...
In your opinion it could also be suitable for input lower voltages working on the dissipation of the Mosfet? I don't know if the inductor could also go into thermal crisis ...
if the thermal problems occurred only on the Mofset a solution I could find (in parallel or heatsink with Thermal Interface) but my doubt is also on the inductor and perhaps on the capacitors (electrolytic input and output)
Eventually, please reccomended an other IC that may be suitable.
Please let me know as soons as possible.
Thanks.Best Regards.