Dear Sir/Madam,
I`m using the ADD5211 to drive a LCD backlight, but sometimes (very rare) it doesn´t power on.
After connecting the EN-pin or the UVLO-pin shortly to ground it starts again.
Unfortunately I didn´t connect the Fault-pin, so I can`t monitor any fault state.
I tried to connect EN-pin or UVLO-pin via a 100kOhm resistor to VIN, but without any success.
I can also reproduce it by permanent powering the ADD5211 and switching off/on the EN-pin.
I already ordered the evaluation board and use quite the same values for all components,
but could not reproduce the faulty behavior.
Production date ADD5211: 1319 @ADD5211-Evalboard and 1634 in my design
Any idea?
Many thanks,
Sven