Post Go back to editing

LDO Voltage Regulator ADP162: use a pull-down external resistor

Hi, I am using the LDO Voltage Regulator ADP162 but I do not find in the datasheet if it is necessary to use a pull-down external resistor in the enable pin. In principle, this enable pin will be controlled by a GPIO pin of the MSP430G2553 MCU. Thank you.

Best regards,
Fran Martin.

  • Hi, Fran.

    It is recommended to put a pull-down resistor in the EN pin. This ensures that the LDO is in shutdown mode and avoids erratic/unpredictable behavior as compared to when left floating. Make sure that the voltage drop cause by the pull-down resistor and the EN leakage (1uA) is less than the EN input logic low voltage threshold (0.4V). In this case, a 10 kohm resistor will do as pull down in the EN pin.

    Regards,
    Errgy

Before You Switch


Switching languages will make ADI Explorer unavailable. Resume your session by switching back to English and reopening ADI Explorer.